I need a 5V, 300 ma from a 24 VDC supply on a PCB. I am confused about PD calculations and theta jA. I am calculating PD as (24-5) x .3A = 5.7 W. Fig 32 0n LM340 data sheet shows max PD vs ambient when mounted on 1 sq in of 2 oz copper and the max wattage is 3.2 W and that is at negative ambient temps.. Less than 2W if the ambient is 25C. How can I get the current I need when the max power is so low. I know I must be looking at this wrong. Can someone help me understand please?
Thanks - John