This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145: Capacitive Load Capabilities

Part Number: LM5145

I'm planning on using the LM5145 as my input buck step-down supply from 40V-60V input to 12V output at 6.5A.  Following this I have several buck regulators generating the various voltage rails needed for my design. each on of those step-down bucks have input caps.  Heaviest of the rails is 0.9V output at 35A.

My question is can the LM5154 function with a large capacitive load?  I've seen regulators function fine until a large capacitive load is applied, then not be able to come up when power is applied.

Thanks,

-j