Can the TPS2400 be used to drive back to back FETs? I need a switch that will hold-off up to 20V from feeding back into the TPS61240 (only rated for 14V) which is used as an OTG supply. The way the circuit is setup, there is a body diode from OUT to IN which is unacceptable in this application.