This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS56339: TPS56339

Part Number: TPS56339

Tool/software: WEBENCH® Design Tools

I designed  TPS56339DDCR  ‑  24V to 5.00V @ 3A with WEBENCH. But i found the tps56339 would be damaged when the input is  above 18V .Both the VIN pin and SW pin short-circuited to GND when the tps56339 is damaged.Could you give some advice please? thank you very much.