This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27750: BQ27750,BQ27742 HDQ communication and protection

Part Number: BQ27750

Hello sir,

may I ask 3 questions about BQ27750,BQ27742 in the application of coulomb-meter?

1. As for HDQ communication,are there some specific recommend for GPIO selection?

2. Could you please provide some drive codes for BQ27750 and BQ27742?

3. whether Battery gauge will happen to electric quantity jump if the battery gauge stays in high temperature or low temperature?

Best regards,

wenting 

  • Hi, Wenting

        For HDQ communication, it is enabled by sending command from I2C instead of GPIO pin configuration.

        For the driver, I think Onyx or Dominik may help on this.

        For electric quantity jump, typically called as SOC jump or Remaining Capacity Jump, could be minimized by optimizing the battery model data stored in the data flash, Onyx can help you for details