Hi Everyone
I'm using a a TPS63000 to provide a 3.5V supply from a Lithium Ion cell.
The cell voltage may be between 3.0 and 4.2 volts so the device may be working in boost or buck.
I'm finding that the current increases to around 800mA even with no load when I reach about 3.2 volts then suddenly drops to almost nothing when I reach around 3.7 volts.
Any ideas why I'm seeing this rise in current ?