Hi Ti team,
My customer is designing the Hi-Fi Audio DAC.
there are using LM27761 to supply Volume IC Vcc(-5V). current output of LM27761 is 60~70mA.
Issue : we can hear noise in the 5-10khz band from the headphone out.
Resolve : Increasing the load to the output of the LM27761 to 150mA eliminates noise.
Increasing the output load eliminates noise, but we cannot add load.
I think the cause of the problem is PFM mode. Can I change PFM operation current? I didn't find any related formulas in the datasheet.
Please check that.
Thanks.