Hi,
I'm choosing the Low noise LDOs.And I want to know the biggest difference between TPS73115-EP and TPS73115.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm choosing the Low noise LDOs.And I want to know the biggest difference between TPS73115-EP and TPS73115.
Thanks.
Hey Eric,
The -EP versions of our devices are a higher grade of our devices.
Below is a list of some of the things -EP has over commercial grade devices:
• Using the latest and most robust plastic encapsulation methodology to support the harsh environment needs.
• Ensuring tin plating content is not above 97% to eliminate the risks related to time-dependent pin-to-pin metal shorts (aka tin whiskers) by assembling the device with NiPdAu plating or SnPb solder balls.
• Using only gold (Au) bond wires to ensure the highest quality die to leadframe connection.
• Performing extended 250 hours highly accelerated temperature and humidity stress testing (HAST) to demonstrate improved moisture resistance, extending both operational life and dormant storage capabilities.
• Extending temperature ranges from -55°C to 125°C to enable the broadest possible use cases.
• Ensuring a single controlled manufacturing baseline flow with a single wafer fab, assembly site and test site to ensure the applicability of customer’s qualification even over multi-decade programs.
• Ensuring orderable (V62/xxxx) DLA vendor items drawings part numbers that eliminate the need specification source controlled drawings.
Thanks,
Daniel