Hi all,
i intend to develop a flyback converter with a single input and two outputs. The outputs must work independently from each other. The input voltage should be in range of 3....5V, the outputs should be in range of 6...7V with a current of 100mA each.
Did have someone an idea which controller can be used for this purposes?
Thanks in Advance.
Alexandru Mixich