Other Parts Discussed in Thread: BQ51013B
We're struggling to deal with dips in the OUT voltage of the bq51003 when there's a load current step from 125 mA to 250 mA. Our system MCU is being reset as a result. We've found that we can add super-capacitors (0.15 Farad) to deal with this, but we have very limited space and the super-caps are too large. We also find that the quoted 90 ms step response is optimistic compared to what we're seeing which is 150 to 200 ms or longer. We're looking for other ideas to try instead of the brute force approach of added bulk capacitance. To that end, here are some thoughts and questions:
- It appears that the bq51003 monitors the voltage on RECT to determine how much power to request from the wireless power transmitter. Is that correct?
- Could the large bulk capacitance on OUT be slowing the step response by masking the load step?
- Is there a way to "pre-load" the system so that the bq51003 requests more power in anticipation of the load step?
- Any other ideas? We can't be the first people to have had this sort of design challenge!
Thanks,
Scott