This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: LED display

Part Number: BQ4050


Hi,

We wanted the LEDs to display State-of-Charge.

I placed LEDs on the PCB in such way, that i have to configure the thresholds:

LED1=40%

LED2=20%

LED3=80%

LED4=60%

LED5=100%

If, for example,  the SOC is 20%, no LED is 'on'.

As i understand, thats because the threshold of LED 2 has to be lower than the threshold of LED1, etc.

Is my assumption is correct?

if yes, is there any way to configure the thresholds of the LEDs  regardless of other LEDs thresholds? 

Best Regards,

Arkadi