Hi
For an application I would like to use the TPS560430 in a flybuck configuration with 1 isolated and 1 non-isolated output.
Since this is my first flybuck design I would like to confirm that the TPS560430XF(FPWM) can be used.
The input is 24V with two ~12V outputs, one isolated. The ouput current for both 12V rails is ~25mA.
The -0.3A negative current limit (FPWM) of the TPS560430XF should be sufficient.
If required I can easily add a bit of load to the output(s) since efficiency is not a concern. The regulation of the isolated output isn't that important.
Due to the low load current I prefer to use DCM if possible.
Can someone confirm the TPS560430XF can be used for this application?
Thanks.