This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030: overcurrent trigger condition and thermal

Part Number: LMR14030


Hi team,

customer test LMR14030 over current protection. customer applicaiton are that:

input 24V ; output 5V

test condition is connect 5V to ground, power up 24V,  they found that the tempature of LMR14030 will be very high, can reach up to about 100C. also, the tempature of inductior and diode will up to 168C.

could you give suggestions about why the LMR14030 tempature very high, does this the normal? what's the over current protection conditions?

thank you.