This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25101: Battery Capacity Status

Part Number: BQ25101
Other Parts Discussed in Thread: BQ27426

Hi,

I know that BQ25101 charging chip is able to indicate whether the battery is in a charging state or non-charging state via the /CHG pin.

My question is:

Can BQ25101 also continuously update the battery capacity status in percentage to MCU, like 90%, 70%, 20% and etc.?

Thanks.