This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62050: Output capacitor, is 15uF possible?

Part Number: TPS62050


Dear TI expert,

I am using the TPS62050 to step down the  voltage from 4AA batteries to 3.3V. I am using a 15uF ceramic input capacitor and currently a 22uF output capacitor. The inductor is 10uH. I am however considering if it is possible to reduce the output capacitor to 15uF. The current consumption of my device is less than 400 mA.

What issues will arise if the output capacitor is reduced to 15uF?

Best regards,

Rune Jacobsen