Other Parts Discussed in Thread: PMP7282, LM555, LM5143-Q1, LM5143
Hi,
I will design a buck converter with two LM5116.I need a high current. Therefore, i will use sync design .
The design I found is 2 phase buck converter(PMP7282 Two-phase buck converter ). I intend to take this design as a reference.
*My input voltage will be single phase dc. What should I pay attention to in sync design for single phase?
*In the dual design I have found, there is a separate EN and UVLO input for both ICs. Are there any pins that can be used in sync design? For example, can EN and UVLO inputs be used together sync design?
*Error comparator designed externally. Should I change?
*The synchronization clock is generated from LM555. However, the phase difference between the two IC's was created (180 degrees). Is this phase difference a design specific to a 2-phase inverter?