Other Parts Discussed in Thread: , TPS3808
Hi,
I would like to detect battery low level event. I am using a 3.7V rechargeable coin battery. The datasheet says "If the voltage on the BAT pin remains above VLOWV, it indicates that the battery is still connected, but has discharged". Moreover the event that signals battery low level is given by internal battery voltage comparator (section 8.3.10.3 of datasheet), but it works for Li-primary battery (CH_EN=0), not for rechargeable batteries.
So how can I detect a battery low level?
Thank you!
Amilcare