Hello community
The controller converts 24V into 5V with a maximum 4.5A output voltage.
Here the circuit:
My question now: How can you improve the circuit further to eliminate this problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello community
Hi Schade:
do you mean even in no load conditon, the mosfet is stil very hot?
1. whether there is short through of high side and low side fet? When high side mosfet turn on and off, whether it will coupling the low side mosfet on? any improve when you add some snubber?
2. it is better to show the SW waveform in 2-4 fsw cycles with low side and high side drive.
3. can you try only reduce the turn on speed of both fet with 10ohm or larger resistor and keep turn off resistor is 0 , see any difference?
Thanks
Daniel Li
We suspect that the high input capacity (CSD87355) is the cause.
We want to try again with the CSD87352 if it is better then.
We had already replaced the gate resistors with 0-OHM resistors, then it got better, but not satisfactorily.
At 1 OHM, the effect already worsens significantly.
Hi Schade:
thank you for your info. Let me know if you need further help
Thanks
Daniel Li