This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: BQ25703A default status

Part Number: BQ25703A

Hi TI Team:

 customer wants to be able to charge the battery in standby mode,but standby mode I2C is not work. Can bq25703a be charged without I2C setting (bq25703a register default state)..

Input 5V ,2cell ,Please Give me Suggst 。

Thanks

CQ.LV

  • Hey CQ.LV,

    The BQ25703A is a host-controlled charger, and thus the charge current and profile must be programmed via I2C by the host.

    In default mode, charging is disabled. The is the EN_AUTO_WAKEUP which is enabled by default, but this will only charge the battery up to the minimum system voltage with 128mA of current.

    Regards,

    Joel H