Other Parts Discussed in Thread: BQ51050B
Hello,
We are actually working on a project and we would like to add a wireless charging functionality. We have chosen the BQ51050BRHLR receveir circuit. However we are new with these wireless charging ICs. We have three main questions :
1) We have checked the BQ51050BRHLR datasheet and we still have doubts how to choose the receiver coil inductance value. I mean do we have to fix a "random" value for the inductance ? Moreover in the datasheet, they talk about Ls and L's. Which one correponds to the receiver coil inductance we have to buy and connect between AC1 and AC2 ? Therefore when we have to chose a receiver coil, do we have to choose it according to its inductance value or DC resistance or both ? We by the way designed the circuit for a 530 mA charging current and the VBAT is a 3.7 V Li-Po battery.
2) So here is below our scheme. We don't know if it's correct and if something is missing without taking account of the missing RX coil.
3) Finally, since we just talked about the receiver circuit, we need a transmitter circuit. Do you recommend any TI transmitter circuit which would be suitable with the BQ51050BRHLR circuit ? In fact we would like if it exists, a board integrating already the transmitter circuit with all the necessary circuits around, so we just have to put the RX coil near the TX coil to start the wireless charging. And how should be the TX coil value comparing to the RX coil one ?
Thank you very much.
Best regards,
Mike