Other Parts Discussed in Thread: BQSTUDIO, BQ34Z100
In the learning cycle you discharge the battery to empty and then let it sit for at least 5 hours which usually turns into 14+ hours over night. During those 5-14 hours you're constantly querying data with bqStudio for the logs so the device doesn't get into SLEEP much if at all. Because of the device's constant drain on the remaining battery in this state I end up with Li Ion batteries draining to under 2V.
It's bad for the batteries. Is it bad for the learning cycle? Is there a way around this problem? What are others doing? Do you power the BQ device externally for this test?