Other Parts Discussed in Thread: BQ25505, , BQ25100
Hi.
Used the BQ25505 to harvest energy from small solar panel mounted on a moving object. Problem is that object constantly gets the panel under different lighting situations.
For this I created a dome type of setup mounting 5 panels facing "all potential" angles so that at least on panel is faacing the the sun +- 15 degrees...
What I totally missed is that I will never get a proper MPPT sample. I guess using MPPT is not in scope for the use case. Then came across the following thread.
Recommending to change to bq25504 to be able to eliminate MPPT all together.
Because of my panel arrangement I have needed to go for 5 separate bq25504 since either serial or parallel arrangements works since no panels are alike from a mounting perspective.
This will cause 5 battery chargers to operate on the same cell. Would a better option be to use 5 separate boost-converters and get them to convert to let's say 5volt and from there connect it to a charger instead to cut down the price of my BOM?? Could you please recommend parts? I guess a really low input voltage is given.
Any benefits of sticking with 5x bq25504??
Thanks!