Other Parts Discussed in Thread: LM5085, , LM5146
Hello,
We were using LM5085 as a battery charger configured for 16.8V output limited at 5A. We had to switch to LM5146-Q1 because it can accept up to 100V, while the LM5085 will only accept up to 75V. As far as I can understanding from using the evaluation board for LM5146-Q1, it is possible to set a current limit that will trip an over current protection -- however this seems to shut off the output current rather than clip it at a specified value.
Is it possible to configure LM5146-Q1 so that it delivers current-limited power? i.e.: when the battery wants to pull 20A at 16.8V it will only get 5A from the circuit.
Respectfully,
-Anthony Andrew