Hello,
I am using the eval board, with the test setup described in the user guide. However, when the enable jumper is turned to ON it looks like there is a short, the input voltage drops from 12V to 2.5V. Current draw is less than 0.5A. I am using a load resistor of 2 ohms (30W). My output voltage jumper is is set to 3.2V. Switching the jumper back to the off enable jumper, the input voltage shows 12 V.