Other Parts Discussed in Thread: PMP20497
Dear Sir, PoE Power Schematic(LM5022).pdf
There is a TI reference design, PMP20497 made by LM5022. I have a question here. I calculated the current passing throguh photo diode (U2), and got 103.4mA [=(54-1.17-1.24)/499], 1.17V is forward voltage of photo diode of U2, 1.24V is the minimum voltage (Vcathod-anode) of U3.
By multipling CTR (=200%~400%) of U2, then getting the current sourcing from U1 pin 3 is 206.8mA~413.6mA. I checked LM5022 datasheet, the maximum souring capability of LM5022 pin 3 is 1.5mA, according above calculation, actually demanding current (206.8mA~413.6mA) is far above 1.5mA, why? Do I make any misunderstanding?