Dear sir
I am using TPS5430 for 7" Monitor with four camera. the operating condtion is as follow
Vin min =12V
Vinmax=30V
Vout=9.5V
I out max=1.5A
but, when enter 17 V input voltage into out product, I can see noise on monitor screen with gray color
and then, we can't see the same noise on monitor screen with the same conditon except 16~18V input voltage
Please tell me how to solve this problem as soon as possible,
Best regards
J.H.Kim