This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27762: LM27762 as constant -5V source

Part Number: LM27762
Other Parts Discussed in Thread: TL072, , LM2772

Hi, all!


I need to read the output of a photodiode through TI Hercules RM57Lx, with the onboard ADC. The photodiode gives a negative voltage, so I have made an inverter circuit using TL072 IC.

The issue is that TL072 IC needs a negative power supply as well. I was using two 9V batteries to provide the +ve and -ve voltages but I need a constant power source. Is LM27762 IC a reliable option?

If not, please, suggest.

Thanks and regards,
Apurv