Other Parts Discussed in Thread: TPS7A45
Hello,
What is the equivalent part for the above part for use in commercial power supplies?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the equivalent part for the above part for use in commercial power supplies?
Anjali,
Can you share your extension only last four digits?
Mitesh
Hey Anjali,
The TPS7A45 has a 01 variant which is the commercial grade version of this device.
Thanks,
Daniel
Anjali,
As Daniel noted, the commercial variant is the TPS7A45 and without the -SP.
However, just to be clear, I want to provide the following information as it may be relevant to your use.
TI cannot share wafer, die and process details specific to any device, as this information is proprietary. Typically there are differences between space and non-space devices (including mil and EP grade products). These differences can be in the form of process, layout, or design changes. These are done to improve radiation performance of space device. Please note that radiation performance for a non-space device can be significantly worse compared to space qualified device even though electrical performance is identical. In addition there are several factors on non-space device that makes it risky for space applications. Some of important factors:
- No single controlled baseline: Translates to high variability of radiation performance (commercial products)
- Mostly use copper bond-wire: May not be reliable for space environment (commercial products)
- No testing for radiation at lot level: High risk of getting devices that have poor radiation level (non-space products)
Regards,
Wade
Thanks Daniel,
I have one more query regarding this:- As I can see from the datasheet that the commercial part number is a 6 pin device with SOT package and the SP part is a 10 pin device in CFP package. Is the device not available in same footprint in both commercial as well as SP part.
Anjali,
The space grade version is available in three variants. Two ceramic packages, and a die only Known Good DIe (KGD).
There is not a footprint that matches the commercial plastic device.
If this answers your question, please click "This Resolved My Issue"
Regards,
Wade