This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I designing LM5022 with LED driver application, based on application note: snva282b and snva229a.
I want to attach additional specification below, is there any reference design or information?
①Open LED detection
⇒Zener diode: D2 is only protection function, I want detect and output signal.
②Monitoring LED current
⇒Sensing Vcs and analog output, is there recommended current shunt monitor?
③Constant current need to adjust linearity, controlling from external analog signal (DAC output from FPGA).
I think that analog signal connect between RFB2 and Q2, is it correct?
Best regards,
Satoshi
Hi Satoshi,
Thank you for designing with the LM5022. Sorry I don't know any existing reference designs for these functions.
If you want to detect LED disconnect: RFB1 voltage would reduce a lot, so you may able to catch it by monitor RFB1 with a comparator.
The voltage across RFB1 represents the LED current.
The circuit achieve constant current. If you want to adjust, you should feed your DAC voltage to RFB1 through a scaling resistor. When you want high current, you need to reduce the DAC voltage.
Hope these help.
Thanks,
Youhao Xi, Applications Engineering