Part Number: TPS709
Hi,
I am asking on behalf of a customer that uses the TPS70933 in a battery powered application to step-down the voltage from 9V input to 3.3V.
When testing, the output of the TPS70933 was connected to a 5V rail through a 10kOhm resistor(with no load on the 3.3V output). This caused an oscillating waveform on the output side. Oscillating between 3.3V to 3.7V and a current of 170uA can be detected through the 10kOhm pull-up resistor. Which indicates that there is a 170uA leakage into the LDO.
We are interested in the internal structure of the device to determine what can cause this oscillation. We know that this is not a recommended way to design the circuit and it will not be a issue in this design.
Do you have any ideas what can cause this waveform? When simulating this scenario in WEBENCH, the fault cannot be detected.