This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Light load efficiency

Other Parts Discussed in Thread: TPS63805

Hi all,

During light load condition, the DC-DC converter are operated in

1. Pulse skipping mode

2. Burst mode.

Of these both mode of operation, which one is more effective and why?

  • Hi Aradhyasambhu,

    Normally, these are two different names for the same mode of operation. The device operates in short bursts, between the bursts it skips PWM pulses. Do you have a particular device on your mind?

    Best regards,
    Milos

  • HI Milos,

    Thanks for the reply. Can you please suggest in which controller they go for both burst mode and pulse skipping method to enhance the light load performance of the DC - DC converter?

  • Hi Aradhyasambhu,

    Do you have specific operating conditions or application in mind, or this is just a general question? If it is a general question, take for example the TPS63805, and check section 9.4.2 of the datasheet. At light loads, the device switches in bursts where it skips the switching cycles depending on the output state of the skip comparator. So you can say it operates in burst mode, or skip mode, or what we call it in this case generically, power-save mode. The names can be different, but they usually refer to the same principle of operation. 

    Best regards,
    Milos