Other Parts Discussed in Thread: BQ25570
Hello,
I am designing an application where a micro needs to be supplied continually. The source is a solar harvesting system and the battery is a Li-Ion battery of 400 mAh. This way, I don´t know if the BQ25570 allows me to supply the micro with 3.3V in the following situations:
- The source is ON but the battery is discharged.
- The source is OFF and the battery is charged.
What I mean is (if it is no well explained),
- What would happen if the battery is discharged and the source is ON? 3.3 V will be in Vout and the battery will be charged?
- What would happend if the battery is charged and the source is OFF? 3.3 V will be in Vout?
Thank you in advanced.