Other Parts Discussed in Thread: TPS28226, TPS28225
Hi E2E,
Good day.
Our customer is looking for the ESD HBM rating for TPS2835.
Thank you in advance for your help.
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Carlo,
Thank you for the interest in the TPS2835. This is an older device and I wanted to see if there is a newer device with similar functions that you might consider.
The TPS28225 and TPS28226 are newer synchronous buck gate drivers that may fit your application. The datasheets can be found in the links below.
http://www.ti.com/lit/ds/symlink/tps28225.pdf
http://www.ti.com/lit/ds/symlink/tps28226.pdf
I did find some data on the TPS2835 ESD testing and the passing results are below.
ESD: 100pF,1500 Ohms 2500 V
CDM 1500 V
Confirm if this addresses your questions, or you can post additional questions on this thread.
Regards,
Hi Richard,
Thank you for your answer. I just want to clarify that the 2500 V is the HBM ESD rating?
Regards,
Carlo
Hello Carlo,
I have reached out to confirm the question regarding if the 2500V is the HBM rating. I hope to hear in the next day or two.
Regards,
Hello Carlo,
I have confirmed the test method and the rating that the results will support.
The test is for HBM rating condition and the test results support a 2kV HBM rating.
Confirm if this addresses your questions, or you can post additional question on this thread.