Hi Team,
The TLV767 package is very small and with a small thermal pad at the bottom. I want to know if you can share the temperature rising vs. current load curve.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
The TLV767 package is very small and with a small thermal pad at the bottom. I want to know if you can share the temperature rising vs. current load curve.
Hi Lenna,
The temperature increase will be proportional to the load current since Tj=Ta+Rja*(Vin-Vou)*Iout. Unfortunately we can't give an exact temperature for your specific application since Rja is highly dependent on the board layout, but we can say that the increase in temperature will be proportional to the increase in current.
If you want to get a better understanding of how board layout can effect Rja, we recently released an app note which evaluated different layouts to see how they affected the Rja parameter. You can find that app note here: http://www.ti.com/lit/an/slvae85/slvae85.pdf
Note that:
Hi Kyle,
Thanks for your quick reply. I know the calculation process. Do you have temperature increasing data based on the EVM?
Hi Lenna,
Unfortunately we don't have specific measurements made on this device, however our EVMs are optimized for thermals with very large amounts of metal and thermal vias connected to the device. We've found that our EVMs perform on par with the "thermally saturated" board shown in the app note I mentioned in my previous post which would result in an expected Rja which is ~54% of the JEDEC number listed in the PDS (Rja=41.8C/W).