Hi
customer want to know, if input voltage is a DC voltage, the output voltage is set higher than input voltage.
can ucc28070 be used as a boost converter?
thanks.
Max Han
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
customer want to know, if input voltage is a DC voltage, the output voltage is set higher than input voltage.
can ucc28070 be used as a boost converter?
thanks.
Max Han
Hello Max,
The UCC28070 cannot be used with a DC input.
The reason for this is that the VINAC signal needs to reset to VINAC<0.7V in order to set the correct multiplier output level.
The input signal needs to be a low frequency AC sine wave
Regards
John