This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: BatteryMode() issue

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO

Hello;

I'm having problems when attempting to set the CAPM bit in the BatteryMode() command. I can successfully read and write from/to other SBS commands...But when attempting to write to BatteryMode (0x03), it won't take.  When I first read it,  I initially get 0x6081, indicating that a "Conditioning cycle requested".  When I write 0xE001, it initially reads back 0xE001...OK.

BUT, when I then reset and run through the configuration routine again, it again, first reads back as 0x6081, and subsequent reads are 0x6001. ??

SO, is there something I'm doing wrong with this SBS command? It doesn't seem to want to be altered.