This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Is there current scaling so that I can use the device with currents above 32760mA?

Part Number: BQ4050

Variations on the BQ device include a current scaling factor so that larger battery packs and currents can be used. I don't see this function on the BQ4050 and I assume that I am missing the right register / command? To get around this problem I have calibrated the system by specifying a resistor is 2X the real value - but is there a better way?

Thanks  in advance.