This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59581: GCLK Calculation and Adjusting Frame Rate

Part Number: TLC59581


Hi Team,

My customer is trying to use the TLC59581 for a matrix display and running into concerns with GCLK, can you help verify a few things for me?

They are doing 8 scan lines and want to achieve 120 frames per second in the 8x8 mode, that would require a GCLK of 257 x 256 x 8 x 120 or about 65.6 MHz, correct? (which I know is double the spec for the chip.)

Assuming my computations are correct, is there a way to increase the frame rate (I’m assuming at the loss of PWM resolution) without running the GCLK at such a high rate?  I would guess that 10 bits of resolution would be enough.

Thanks,

David