Hi,
We use a Battery which will present 0V to the charger when it has been discharged below 3.0V (self disconnecting)
The Inbuilt Battery Protection needs at least 3.0V to be present to re-activate the Battery Connection to begin charging.
We would like to charge with a max current somewhere between 0.8A and 3A
We have an input voltage of 5V (in one case 20V would be useful too)
Does anyone know which Switching Battery Charge ICs can be used for this purpose?
Cheers
-Glen