There seems to be some confusion in the documentation regarding the backup state and capabilities of the TPS659xx family.
Document SWCA025 states on page 1:
"The TPS65930 and TPS65920 devices have the same backup state functionality as
TPS65950 device. Hence the backup state functionality described for TPS65950 in this
report also applies to TPS65930/20."
This seems clear and unequivocal. However, document SWCU052A states on page 211
"BACKUP System is powered only with backup battery and maintains only VBRTC supply.
Note: This state is inherited from the TPS65950 device and is not appropriate for
the TPS65930 or the TPS65920, because they do not accept the use of a backup
batter."
Also, document SWCU052A states on page 217:
"No events put the TPS65930 and TPS65920 in BACKUP state, because these devices do not have
access to a backup battery."
Both these statements are in conflict with the other document, so what am I to believe? It does not seem to make sense that the devices would have an RTC that cannot be backed up. I require this capability, but do not require all the other additional functionality of the TPS65950. Also, both the TPS65930 and TPS65920 have a BKBAT pin, which I assume is the pin by which the devices is connected to the backup battery (documentation not very clear) so what use is it without this functionality?