This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
About TI Designs: TIDA-01546 Battery and System Health Monitoring of Battery-Powered Smart Flow Meters Reference Design
http://www.ti.com/lit/ug/tidudo5a/tidudo5a.pdf
I have some questions to consult.
PAGE 13
3.2.1.1 Steps to Calibrate bq35100
一、SYS_GND is PACK–?
from TIDA-01546 Schematic and Block Diagram, I think is.
二、
2.3.2.1.1.2 Hardware Connections
2. Connect the battery to J3 terminal block (BAT+, BAT–).
3. Connect the load to J3 terminal block (BAT+, SYS_GND).
In 3.2.1.1.3.2 Current Calibration
6. Verify whether the current reports 0 mA.
7. Connect a 1-A load from BAT+ to PACK–
Board Offset/CC Offset calibration need Verify whether the current reports 0 mA. the 0mA means load 0mA?
Connect the load to J3 terminal block (BAT+, SYS_GND)
——if I connect 0 mA load means the current reports 0 mA?
please tell me how J3 connect to finish Board Offset/CC Offset calibration in TIDA-01546?
thank you!
Hi Zhangtao
There should be no load connected to J3. Just connect your battery to bat+ and bat_ and click the calibrate cc offset and board offset function under the calibration tab of bqstudio.
Thanks
Onyx
hello Onyx,
could TI Designs:TIDA-01546 tested Lithium Thionyl Chloride (Li-SOCl2) battery EOS mode?
Is there tested data can share me ?
I want to look TI EOS mode`s correct test data.
I want to konw the how are ScaledR measuredZ SOH changed?
it`s trend。then I can check my data and debugging。
thank you!
hi
All the documents that is available for that reference design is online. We don't have further documents to share at this time unfortunately.
thanks
Onyx