This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for recommendation for stand-alone, easy to use 1s Li-Ion/Li-Po battery management

Other Parts Discussed in Thread: BQ25606

Hello,

We are helping a client with a portable consumer audio device. They have chosen this battery. I am looking for a very small (the PCBA is same size as the battery) charging/gauging/protection solution. It needs to be hardware controlled (i.e. standalone) and easy to use. It will charge from a standard USB connector.

Is there an integrated IC that contains this functionality in a single device? Is there a solution that integrates back-side Buck/Boost converter to generate the 3.3V we need?

Would you please provide a recommendation for this application?

Thanks in advance,

Cody