Hi,
can you please tell me is this inductor suitable for use with TPS560430-Q1 for 0-600mA load?
Inductor: 8.2uH from https://www.coilcraft.com/pdfs/mss6132.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
can you please tell me is this inductor suitable for use with TPS560430-Q1 for 0-600mA load?
Inductor: 8.2uH from https://www.coilcraft.com/pdfs/mss6132.pdf
Inductor value determines stability.
Inductor power capabilities is determined by DC current and peak current limit of device.
Please provide more information regarding input/output power and desired switching frequency.
Hi Marshall,
the Vin is 9-15V, Vout is 3.3A. Max current is 600mA. The TPS560430-Q1 would be used in PFM mode and the frequency is 2.1 MHz.
Upon further searching I found this inductor which I think would fit in my application, and is smaller than the one in my initial post: XGL4020-822ME. The datasheet is here: https://www.coilcraft.com/pdfs/xgl4020.pdf
Can you please confirm the XGL4020-822ME is suitable for my application?
You will have reasonable ripple <30% with value
Your inductor choice looks good after examining datasheet.