Other Parts Discussed in Thread: BQ77905
Hi,
we are working on bq77915 for battery protection. we have a 3s configuration. Instead using pack -ve terminal to connect the load, can the load -ve terminal be connected between the Fet drain terminals? we want to add a functionality to our design where the load is given high priority when the adapter is connected to the system ( Eg: if the load and adapter are connected to the system, the load load should be met by the adapter).
Is there any way to achieve this functionality ?
Thank-you