This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23610: Cout and Inductance

Part Number: LMR23610


Hi, Team.

I've been asked by Customer to know recommended value(L and Cout) for below required spec.

Vin:16.5V

Vout:5V

Iout:30mA

<Inductance>

As my calc, the below value looks ok but customer want to make sure how much value recommended from BU to select their inductance selection.

*50% current ripple is assumed.

193uH=(((16.5-5)/(0.03*1.5))*(5/(16.5*400*10^3)))

<Cout>

they want ripple on Vout would be within 100mV.

i believe that Cout(47uF) is good choice from datasheet. what do you think?

(Cout must be higher than 3.1uF and its ESR must be below than 100mOhm, correct?)