Do you have any DC/DC to offer with the same footprint of TPS63070 that can work with ultra-low operating quiescent current0 (7-11 µA)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ron,
I split the original thread, since it was marked as resolved.
We do not have a low-Iq TPS63070 alternative, for input/output voltages above 5.5 V.
Could you please confirm what are your Vin, Vout, Iout requirements? In your original thread you mentioned that your input voltage is 4 V and the output voltage is 5 V. If so, the TPS63802 would be a better match, it is in similar package as the TPS63070, but with lower Iq.
Best regards,
Milos
Hi Milos,
Vin = 2.5~5V
Vout = 4V
Imax = 1A
Iq = as low as possiable (10uA or less)
in the datasheets, it seems the TPS63802 and TPS63070 has a diffrent package.
TPS63802 has a "10-Pin VSON-HR" package while TPS63070 has "VQFN-15".
Hi Ron,
The TPS63802 would fit better than the TPS63070.
Yes, these are not pin-to-pin compatible devices. Can you still work with it? They have similar DFN/QFN packages, and similar pin arrangement, so the PCB redesign should not be too difficult.
Best regards,
Milos
Hi Ron,
Yes. There might be a package from another manufacturer that has the same size and pin spacing, but the pin arrangement (and therefore the footprint) is unique, since some pins are thermally enhanced.
Best regards,
Milos