This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606A-Q1: Can I use for LiFePO4 it?

Part Number: BQ79606A-Q1

Dear TI-er.

Can I use for LiFePO4 it?

plz help me.

  • Hi Kiyong,

    Yes, LiFePO4 cells can be supported by the bq79606A-Q1. Please see the recommended operating conditions table in the datasheet (section 7.3) and ensure that the Vcell/Vmodule specs will be met and note that a 2V min is required for using the internal cell balancing FET. 

    Regards,

    Taylor