This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616: Can the safety timer be longer if I used 0.1uF +/- 20% plus the 10% accuracy on the TTC pin

Part Number: BQ24616

Regarding the bq24616 safety timer, te datasheet states the maximum to be 10 hours. Can the timer be more than that if you I used 0.1uF +/- 20% plus the 10% accuracy on the TTC pin?

Also, what is the recommended capacitor at the TTC pin if my battery chargers in 3.5 hours at 25 degree C?

 

Thanks,

Lauren