This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC7705M: About the operating conditions of TLC7705M

Part Number: TLC7705M

Hello

My customer wants to use TLC7705M under the following conditions.

VDD = 3.3V
SENSE input = 5V (monitoring an other power rail voltage)

Can it be used according to customer requirements?

However, RECOMMENDED OPERATING CONDITIONS in the data sheet (p.5) is as follows.

VI (input voltage): 0V (min), VDD (max)

This is inconsistent with customer requirements.
However, it seems to be usable from the internal block diagram.
So please let me know if the SENSE input can be used without following the recommended operating conditions (VI: input voltage).

Best regards,
hashi