Hi Team,
pls recommend the most suitable solution for buck boost for below condition,
1. Vin min~3.5V
2. Vin max ~ 15V
3. Vout 3.5~5V
4. Iout max 2.5A~3A
5. switching frequency > 1MHz
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
pls recommend the most suitable solution for buck boost for below condition,
1. Vin min~3.5V
2. Vin max ~ 15V
3. Vout 3.5~5V
4. Iout max 2.5A~3A
5. switching frequency > 1MHz
thanks!
add more critiria,
1. Vin min: < 3.5V
2. Vin max: > 15V
3. Vout can cover from 3.5V to 5V
4. Iout max: 2.5A to 3A
5. switching frequency > 1MHz
6. Good thermal resistance (junction to ambient) < 70degC/W
7. good line/load transient response
6. Small package
Hi Bonnie,
The closest fit is the TPS63070.
Best regards,
Milos
Hi Milos,
For the point #4, let me be more specific.
Our Vout is planned to set at 3.7V. Also, the Vin may range from 3.5V to 5.25V, due to power cable loss or compatibility for different power adapter.
Could TI give a promise that with Vin from 3.5V to 5.25V, the Iout can always work more than 2.5A?
Hi Bonnie,
Then I will repeat the measurement specifically for Vout = 3.7 V. At this output voltage I think it will be tight, and the maximum output current will be somewhere between 2 A and 2.5 A. But I will let you know today.
In the meantime, just two additional notes, let me know if you have comments for these:
Best regards,
Milos
Hi Bonnie,
At Vin = 3.5 V, the TPS63070 can support at most Iout = 2.2 A. For Iout = 2.5 A, you need at least Vin = 4 V.
Is the output current continuous or in short pulses?
Best regards,
Milos
Hi Bonnie,
We haven’t heard back so we're assuming this resolves your issue. If not, just post a reply below, or create a new thread if the thread has locked due to time-out.
Thanks and regards,
Milos